2020-03-16 6:45 AM
Hi,
I'm developing an application with freertos that starts from the address 0x08004000 instead of the standard 0x08000000, because at the start address I have a bootloader but I'm not able to debug the application. I changed the VTOR offset to 0x4000 in the startup file generated by the internal cubeMX, and I also added the following line in: startup - "Initialization Commands" of the debug configuration
set *0xe000ed08 = 0x4000
set $sp = *(unsigned int*)0x4000
set $pc = *(unsigned int*)0x4004
tbreak mainI'm using jlink or in alternative stlink_v2 but nothing changes. The code is loaded always from address 0x08000000.
Someone could help me? These settings are enough to debug a freertos application?
Thanks in advance
Solved! Go to Solution.
2020-03-16 1:02 PM
2020-03-16 1:02 PM
set $sp = *(0x08000000 + 0x4000)
set $pc = *(0x08000000 + 0x4004)
2020-03-17 2:02 AM
thanks a lot, it's correct.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.