2025-12-19 5:42 AM - last edited on 2025-12-19 5:52 AM by Andrew Neil
Today I started STM32CubeIDE again, was notified that an update is due, installed the update (2.0.0). Got an error alert "Computing 'size'", and the Info startup said "URL not found". Anyway, ignored this, started to build my project again. I added ADC1 (before I did the update), but didn't compile that with the old version of Cube. Now the first compile under the new version fails, saying :
../Drivers/STM32H5xx_HAL_Driver/Inc/stm32h5xx_hal_adc.h:1981:67: note: expected 'const ADC_HandleTypeDef *' but argument is of type 'ADC_HandleTypeDef'
1981 | uint32_t HAL_ADC_GetValue(const ADC_HandleTypeDef *hadc);
| ~~~~~~~~~~~~~~~~~~~~~~~~~^~~~
Solved! Go to Solution.
2025-12-19 5:48 AM - edited 2025-12-19 5:50 AM
You've passed the handle itself, but the function requires a pointer to the handle.
PS:
Here's some instructions for posting formatted text which is not source code - such as compiler output.
2025-12-19 5:48 AM - edited 2025-12-19 5:50 AM
You've passed the handle itself, but the function requires a pointer to the handle.
PS:
Here's some instructions for posting formatted text which is not source code - such as compiler output.
2025-12-19 5:51 AM
Ah, silly me. I didn't care when using autocompletion (CTRL-Space). Thanks. Is working now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.