2023-03-17 8:14 AM
For the STM32U575 SFRs in STM32CubeIDE, the LPTIM1 DIER_output has a CC1IF instead of CC1IE.
Also what is the difference between DIER_output and DIER_input ? And why are there bits name different ?
Solved! Go to Solution.
2023-03-20 8:36 AM
Internal tickets number: 147961 (This is an internal tracking number and is not accessible or usable by customers).
Regards
DianeP
2023-03-20 8:12 AM
Hello @Community member
After check on my side , i confirm that we have errors in SFRs of STM32CubeIDE.
The difference between LPTIM1 DIER_output and LPTIM1 DIER_input is :
LPTIM1 DIER_output ( Output cature Mode)
LPTIM1 DIER_input ( Input cature Mode) :
2023-03-20 8:15 AM
LPTIM DIER_input : as soon as we receive an event on Input, we store the value of the LPTIM counter in the capture register.
LPTIM DIER_output: A value is stored in the LPTIM capture register and as soon as the counter reaches this value, an interrupt is generated .
Regards
DianeP
2023-03-20 8:26 AM
Thank you for the answer.
2023-03-20 8:36 AM
Internal tickets number: 147961 (This is an internal tracking number and is not accessible or usable by customers).
Regards
DianeP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.