2020-02-19 12:56 AM
I am trying to create a custom bootloader and having trouble debugging where in the application it jumps to.
Both projects are in the IDE.
If needed. The MCU I use is a STM32F103RET6
2020-02-19 3:07 AM
Better do it with a much simpler and better approach compared to a typical one from ST's examples. Look for my comment here:
2020-02-20 3:33 AM
I have seen the example but I cannot figure out how to implement it myself.
My experience with assembly is none
2020-02-20 5:58 AM
Not using CubeIDE here, but should be able to at least step across the transition in a disassembly view. Make sure it is getting to the right place. Use the .MAP file from the linker to understand where Reset_Handler, main, etc are situated in the application image.
Perhaps look at IAP (In-App Programming) examples.
If the clocks and PLL are already up, I would not perform that step again. Make sure the vector table is set in SCB->VTOR correctly, check SystemInit(). Ideally have a UART working so you can output some telemetry as you leave loader and enter application.
>>My experience with assembly is none
Might want to get a better understanding of how the MCUs work, it will help with the implementational detail, and following what's happening.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.