cancel
Showing results for 
Search instead for 
Did you mean: 

Couldnot reconstruct chunks at receiver end

shaik_simran
Associate

Hello!

I am doing a project using STM32cube ide , the problem I am facing is at the receiver end when the data at the transmitter is transmitted in form of chunks but at the receiver end, the received data could not reconstruct , the receiver is taking 4 sec to switch and send acknowledgement that the packet is received successfully. Can Someone suggest what should I do further to achieve the data reconstruction and receive acknowledgement.  

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Andrew Neil
Super User

You need to give a lot more detail for anyone to have any idea what you're talking about

 


@shaik_simran wrote:

at the receiver end .  


What "receiver" ?

 


@shaik_simran wrote:

the data at the transmitter is transmitted in form of chunks .  


What "data" ?

What "transmitter" ?

What are these "chunks" ?

 


@shaik_simran wrote:

at the receiver end, the received data could not reconstruct , .  


Why not? Are the "chunks" corrupted, or what?

 


@shaik_simran wrote:

the receiver is taking 4 sec to switch and send acknowledgement that the packet is received successfully.  


Is that problem? If it is, then why is it a problem? What does it have to do with the failure to reassemble "chunks"?

 


@shaik_simran wrote:

Can Someone suggest what should I do further to achieve the data reconstruction and receive acknowledgement.  


Not without a lot more detail from you!

  • What, exactly, are you doing at the moment?
  • What results were you expecting?
  • What results are you actually getting?
  • What investigation/debugging have you done to find the problem(s)?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

@shaik_simran wrote:

the receiver is taking 4 sec to switch and send acknowledgement that the packet is received successfully. .  


Is this related: https://community.st.com/t5/stm32-mcus-wireless/want-to-establish-a-full-duplex-communication-between-two/m-p/677327/highlight/true#M19185 ?

:thinking_face:

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.