2024-01-31 3:33 AM
Hi
I am using STM32F446ZET6 board but I am unable to generate code. I am facing this issue "Code generation could not be done most probably because the necessary firmware package is missing" I have tried all the process which are mentioned on different platform even on ST community page. I tried to download the firmware package manually and installed it but the error is same. kindly tell me what should I do. STM32CubeIDE version is 1.14.1. and firmware package version is 1.28.0. but nothing is working after every possible solution.
2024-01-31 5:20 AM
Hello @SShah.27
First let me thank you for posting.
In order to overcome this problem please follow those steps:
- First make sure that your STM32CubeIDE is connected to the Internet:
More details could be found in UM2609 section 1.2.3 STM32CubeIDE user authentication.
- Try to uninstall then reinstall STM32CubeIDE .
I will be waiting for your feedback.
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-31 6:16 AM
Go into Help -> Manage Embedded Software Packages and install the necessary firmware package.
2024-01-31 9:52 PM
Hi Guru
Thank you for your answer but I have tried this solution as well but in my case its not working.
2024-01-31 9:53 PM
Hello Ghofrane
Thank you for your reply i have connected my stm32cubeide to the internet. also i have uninstalled and installed but its showing same error.
Thnx
2024-01-31 11:59 PM
Hello @SShah.27 ,
I assume you start a project from STM32 Target Selector using Board NUCLEO-F446ZE, right ?
If the code generation tells you the firmware is missing, then the first thing to check is your firmware repository path settings.
Open menu Window > Preferences, then in the window select STM32Cube > Firmware Updater, and check the field Repository Setup. Click Browse to open the selected folder and check its contents for the STM32F4 pack you are using.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.