2023-06-27 3:18 AM
Hi,
I'm following the LoRaWAN with STM32 Getting Started series on youtube and stuck with Part 6 - Low power modes. I need to change the "DEFAULT_TX_POWER" to TX_POWER_11 to work with the X-NUCLEO-LPM01A Shield.
I'm unable to make any changes to the region.h files in STM32Cube-fw-wl-v1.3.0. (Or any of the header files found in Middlewares/Third_Party). Is this normal and I just have to create new head files or am I missing something?
Kind regards,
Oliver
Solved! Go to Solution.
2023-06-27 5:44 AM - edited 2023-06-27 5:45 AM
Hi @ollyole,
Sometimes some files are read-only to avoid modifying some libraries by mistake. To change this you can modify the properties of the file.
If you are on windows, right click on the file (in the file explorer), then go to properties and under the general section you can uncheck read-only.
On Linux open the console and use the command :
chmod u+w name_of_your_file to enable write permission.
This should solve your file editing problem. If it persists, tell me and we'll look together where it can come from.
Best Regards,
Florian LR
2023-06-27 5:44 AM - edited 2023-06-27 5:45 AM
Hi @ollyole,
Sometimes some files are read-only to avoid modifying some libraries by mistake. To change this you can modify the properties of the file.
If you are on windows, right click on the file (in the file explorer), then go to properties and under the general section you can uncheck read-only.
On Linux open the console and use the command :
chmod u+w name_of_your_file to enable write permission.
This should solve your file editing problem. If it persists, tell me and we'll look together where it can come from.
Best Regards,
Florian LR
2023-06-27 6:57 AM
Thanks Florian! Now changed and able to see and change the power consumption :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.