2025-11-25 4:29 PM - last edited on 2025-11-25 7:06 PM by TDK
STM32CubeIDE Version: 2.0.0
When trying to create a new project from the IOC of another project, I can't find a way to do it. Is this feature lost or BUG ? Thanks in advance.
Solved! Go to Solution.
2026-01-27 2:31 PM
@fpgiovanini You may find it more productive to approach the subject with the assumption of good faith.
Here are a few topics which cover the rationale:
STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community
STM32CubeIDE 2.0.0 released - STMicroelectronics Community
2025-11-25 7:06 PM
STM32CubeIDE doesn't open or deal with IOC files anymore. Use the standalone STM32CubeMX to open the IOC, save it somewhere else, and create a project.
2025-11-25 8:56 PM
Thanks for the reply. Do you know where I can find documentation for this procedure? I want to keep the configuration from previous projects. They even removed the asterisks (which showed the most frequently used MCUs) when creating a project and made everything more cumbersome, with a smaller font than before...
2025-11-26 4:11 AM
@yogui_ricardo wrote:Is this feature lost or BUG ?
The CubeMX functionality has been separated from CubeIDE v2.0.0:
2025-11-26 6:18 AM
Here's procedure:
Open IOC file in standalone STM32CubeMX.
Select File -> Save Project As and save it at another location.
Generate Code. Select Open Project on popup after code generates.
2025-11-26 6:39 AM
I managed to get it working last night, starting from the MX and it opens the IDE, with or without IOC... perhaps in habit one loses the ability to see the advantages of changes... in any case, I think I prefer integration over interoperability, thanks and regards
2026-01-27 2:31 PM
@fpgiovanini You may find it more productive to approach the subject with the assumption of good faith.
Here are a few topics which cover the rationale:
STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community
STM32CubeIDE 2.0.0 released - STMicroelectronics Community
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.