2022-12-12 9:49 AM
I am currently working on a project that will use a STM32L452VET3 when the product is deployed. The PCB for the product is still being laid out, so in the meantime, I have a Nucleo board that has an STM32L452RET6 that we will use to develop and test the embedded application.
Given that the two MCUs are of the same family, I don't want to have two separate projects that are 99% identical, but I need to keep an .ioc file for both devices. Is there a way to have the .ioc output to the same Drivers/Core/Middleware directories and then conditionally compile for one target or the other (or something to that effect)?
Thanks in advance.
2022-12-12 4:55 PM
Create several project configurations that have preprocessor definitions, maybe some different modules per target, etc.
> Is there a way to have the .ioc output to the same Drivers/Core/Middleware directories
No, the Cube does not support this directly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.