STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Sharing .c/.h pairs in Multiple Projects(Mainting .c/.h files whilst they are in development across multiple projects)

Hi,First post here. I've been using Eclipse previously with SystemWorkbench for STM32 and now the STM32CubeIDE.I'm working on an embedded project which uses multiple microcontrollers and need to use the same .c and .h files for both (with different c...

SSpen by Associate II
  • 4775 Views
  • 7 replies
  • 0 kudos

Target is not responding, STM32 NUCLEO-F446RE

I apologize about this, I am very new to this micro-controller and this programming language. I have no idea how to move forward with this. Thank you in advance!/* USER CODE BEGIN Header */ /** ******************************************************...

Aaronium by Associate III
  • 2749 Views
  • 6 replies
  • 0 kudos

[STM32CubeIDE] Please add the IDE version in the next versions

When someone does a tutorial, it is possible that the person will forget to show the version of the tool.So if it is possible to show the software version along with the window title, it can be useful for tracking in the future, when someone else is ...

0690X00000DYOBrQAP.png
by Not applicable
  • 663 Views
  • 0 replies
  • 1 kudos

STM32CubeIDE migration to 1.3.0 appears to break debugger

Hi there!Each project I've migrated from the previous version of STM32CubeIDE to 1.3.0 can no longer debug properly.When launching a debug session I now always get the following:But if I create a new project from scratch everything is fine.Is anyone ...

0690X00000DYNMyQAP.jpg
etheory by Senior II
  • 1867 Views
  • 3 replies
  • 1 kudos

could not convert atollic project into stm32cubeide

I checked some solutions in this community, but mine is special, there are totally no convert log produced, not response, no popup, no error message, I followed https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/ef/c8/90/3d...

0690X00000DYMe8QAH.png 0690X00000DYMdZQAX.png 0690X00000DYMdeQAH.png
adam.wu by Associate II
  • 1484 Views
  • 1 replies
  • 1 kudos

Debugging when using the external loader for QUADSPI FLASH

I am looking for some input on this.When debugging while using an external loader for the QUADSPI FLASH, why does the debugger not start at the breakpoint in main.c like it does when not using the external loader? In fact, there's no way to "Resume" ...

scottSD by Lead
  • 1291 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.