STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

FreeRTOS and SEGGER SystemView not working

Hello,I am trying to get FreeRTOS and SEGGER SystemView (3.1) to run on an STM32F103RCTx. I used the appropriate manual from SEGGER to include all the necessary folders in my project. Although I have included all the new folders in the Include Paths ...

0690X00000DCBtNQAX.png 0690X00000DCBv0QAH.png

Resolved! Cann't parse large string on STM32F746VGTX with cJSON

Hi all,I'm trying parse a large string stored on internal flash (up to 100 KB). Error is occurred around 60 KB.I tested the same string with cJSON on Visual Studio, and it work well.I think the problem is mcu doesn't have enough heap ram for cJSON.I ...

0693W000000Tc0RQAS.png

Can't install MCU packages

After choosing Help→Manage Embedded Software Packages and selecting from the list F3 package I get "Error downloading the file" (more details in attached picture). Tried downloading the file manually and installing using local copy, but also get an u...

AVenc.16 by Associate
  • 1555 Views
  • 1 replies
  • 0 kudos

STM32Cube - dark colour mode

Hi everyone,how can i change the stm32Cube to Dark mode (black background) without change every single colour? If i change only background -> some letters will unvisible because it's black yet. So i have to change (and find out a optimum ;) many seet...

TThie.1 by Associate II
  • 7655 Views
  • 3 replies
  • 2 kudos

I am a student intern, new to embedded programming. I am trying to learn using the STM32L476 Discovery board. I was trying to the basic blinky code test, and I am unable to to do so properly

No matter which LED port/pin i toggle, only one specific LED blinks. Also, the time delay in the code is not reflected. It would be great if someone can please help me out with this

Divya by Associate II
  • 1343 Views
  • 2 replies
  • 0 kudos

Resolved! How do I enable FreeRTOS debugging support in CubeIDE?

I've just started my first FreeRTOS-based project. In the debugger, when I pause execution, all I see is this stack trace:Thread #1 [main] 1 [core: 0] (suspended : Signal : 0:Signal 0) prvCheckTasksWaitingTermination() at tasks.c:2,488 0x800b4f4 ...

CDew.1 by Associate III
  • 2033 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G070 PWM polarity register is changed

Hi,I use HAL library to build code in CubeIDE. I use TIM1 channel 1 and 2 to output PWM.Channel 2 is changed pulse value to change PWM duty. When I repeat to set up this value. Sometimes, the register CC2P will be changed. But, I don't change polarit...

BPai.1 by Associate
  • 1108 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.