STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

I couldn't update STM32CubeIDE to 1.3.1

This is the error I encountered. A colleague was able to successfully update.Any ideas why I encounter this problem?An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal....

MFend by Associate III
  • 2203 Views
  • 4 replies
  • 0 kudos

Could someone write how to do GPIO without HAL?

I saw somewhere a very basic examples how to do basic GPIO. But now I can't find it. Most of my bookmarks for this forum do not work anyway, all though they not are so old.But could some one write examples of how to write or read one pin or several a...

LMI2 by Lead
  • 5102 Views
  • 8 replies
  • 0 kudos

Resolved! How to download code to FLASH Memory Bank 2 using STM32CubeIDE

Hello, everyone.When downloading the code using STM32CubeProgrammer, I was able to download the code to the location I wanted by specifying the start address.What I'm curious about is how to set up to download to where I want to be when I debug and d...

Ekim.1 by Associate II
  • 2518 Views
  • 1 replies
  • 0 kudos

cubeide can not choose firmware package

hi, I am using cubeide v1.3 on win10.While I am trying to generate code automatically using cubeide, I found I cannot change the firmware package name and version.Since I only installed STM32CubeFW_F4 V1.24.0, and I donot wanna update to the newest v...

spica lai by Associate II
  • 8570 Views
  • 9 replies
  • 0 kudos

Migration from TrueSTUDIO to STM32CubeIDE, missing icons.

I just migrate a project from TrueSTUDIO to STM32CubeIDE. I am quite disappointed, the compilation and launching of the debug are twice as long. How is it possible ? This does not go in the direction of progress.How to recover the very practical icon...

0693W000000VsrLQAS.png

where is internal register

Hi . first of all is there any complete resource for all feature of stm32cubeIDE?Second of all in keil in debug mode we have a part for internal register of processor which show us the operating mode of processor for example thread or handler mode (a...

0693W000000VoVfQAK.png
M N by Associate II
  • 1033 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.