STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can two DMA work in parallel without competing for Bus?

Hi, I was wondering if the two DMA modules can work simultaneously without competing for Bus?For example:In BusMatrix.png file you can see that both DMA1 and DMA2 are connected SRAM1,SRAM2,AHB1 peripherals and AHB2 peripherals.So if I set the DMA1 to...

LLOLO.1 by Associate II
  • 6222 Views
  • 9 replies
  • 0 kudos

Resolved! CubeIDE: Build fails (make: returns with error 2)

HiI try to build a small project (only timer interrupt triggered led blinking) to get familiar with the basic tools. But CubeIDE quits a build with following:08:47:42 **** Incremental Build of configuration Debug for project SandkastenF3 **** make -j...

OLenz.1 by Associate II
  • 5083 Views
  • 5 replies
  • 0 kudos

Can I use FIFO without enabling DMA in STM32?

I want to use FIFO without Enabling USART_DMA in STM32CubeIDE . Is this is possible? If possible I can differentiate the small delays between data. and I can process the data according my requirement.

Mr.L0seR by Associate II
  • 2549 Views
  • 4 replies
  • 0 kudos

How to exchange MCU?

What is the best way to change the MCU in an existing project, for example if the memory has become too small and i want to switch to the same MCU with more memory?Do you really have to start all over with configuring the pins, adding compiler settin...

Problems with downloading program.

Hello,if I try to download my program from STM32CubeIDE, the following will happen:STMicroelectronics ST-LINK GDB server. Version 5.2.3 Copyright (c) 2019, STMicroelectronics. All rights reserved.   Starting server with the following options: ...

0693W000001sheGQAQ.png 0693W000001sheLQAQ.png
Moritz1 by Associate III
  • 1614 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.