STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STD peripheral and Hal driver

Dear ST Hello,What is the deference between Std peripheral drivers and Hal drivers please?Some project use the std peripheral and IDE cube uses the Hal drivers, could you please clarify this point?Thank you in advance,S.Tarik

Installation stm32cudeIDE

I am new to the use of STM32cudeIDE. when i tried to create my first project , following youtube videos , when i choose the board i saw the above error. How to solve this error ?? I need any advice

0693W000001tObZQAU.png
CQwer.1 by Associate
  • 1175 Views
  • 1 replies
  • 0 kudos

Hex file generated in release mode doing malfunction

HI all, I'm using STM32L073 MCU and STMCube IDE (Version: 1.1.0) for a project, facing a strange situation when I'm flashing hex generated in release mode, it started doing malfunction, whereas while flashing MCU directly from IDE in release mode its...

I finished my project, how do I license it?

Forgive if this is an obvious question but I'm new to software programming and I'm not familiar with licensing in general. I finished my project using STM32CubeIDE and I want to release my work under GPLv3 license. The issue is that my own code is ju...

LIORI.1 by Associate
  • 773 Views
  • 0 replies
  • 0 kudos

SMBUS driver not working STM32F446

Hi there...I'm trying to read(in blocking communication) battery related parameters on 2 wire SMBUS on a battery through Nucleo-F446ze and also on a custom board with stm32f446vc, but only interrupt "HAL_SMBUS_MasterTxCpltCallback" triggering, but no...

JChou.1 by Associate III
  • 1032 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE build (Make) incredibly slow

Hello, I created a project with many C files (around 50 or 60) and the build is incredibly slow. I'm just doing "build project", and even when nothing changed in the project, it takes several MINUTES just to start compiling the few modified C files.T...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.