STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

"StringOut" works while "printf" doesn't.

Hello,I'm working with the NUCLEO-F722ZE EVB on STM32CubeIDE.In my code I tried to make the "printf" function work.I used the procedure described in this video:https://www.youtube.com/watch?v=9ntZ3dwGsMkIt basically involves adding this code (the ful...

skon.1 by Senior
  • 2474 Views
  • 5 replies
  • 0 kudos

Two CubeIde instances with two Debugger

Hello all,I have a SPI project: One Nucleo Board = SPI Master, Another Nucleo = Slave.I want to debug both boards (onboard STLink) at the same time by running two instances of CubeIde.Problem: both STLink listening to the same port on my PC. When one...

OBorg.1 by Associate III
  • 2259 Views
  • 2 replies
  • 1 kudos

Resolved! How to update CubeIDE from 1.3.0 to 1.3.1 instead of 1.4.1

Hi,all my co-workers work with CubeIDE 1.3.1 (with embedded MX 6.5.1). Because we share our projects I want to install the same version of IDE and MX.I already install CubeIDE 1.3.0 (which i found on ST site) and try to update it to 1.3.1.But only ve...

grzeslawm by Associate II
  • 2286 Views
  • 4 replies
  • 1 kudos

Resolved! How to Install F0 Examples to CubeIDE

Hello,I would like to select STM32F0 examples projects from the New Project -> Example Selector.I have CubeIDE, and in the MCU/MPU selector I can select my NUCLEO-F072RB. In the Example Selector I can see examples for STM32 F4, F7, G0, G4, H7, L5 an...

VKais.1 by Associate II
  • 3281 Views
  • 2 replies
  • 2 kudos

Just getting started with CubeIDE and am working with an existing project, but having an issue with flashing the code to the target.

Ubuntu Linux 20.04 and error is Program file does not exist. /home/burtbicksler/ExtraDrive/STM32CubeID/workspace_1.4.0/FD-JUL-MB/Debug\FD-JUL-MB.elf not foundThe elf file DOES exist but it looks like the IDE is putting a backslash after the Debug di...

BBick.1 by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos

Resolved! Error in final launch sequence: Failed to execute MI command: symbol-file "C:\\Workspace\\STM Motor Control\\DCMotor\\DCMotor.ioc"

Hi,I'm trying to debug STEVAL$STSPIN3202 motor control board. I have generated code by using motor control workbench. I compile the code without anyproblem, but i recieve attached error message.I'll be glad to get your support.thanksMustafa

MTARH.1 by Associate II
  • 3551 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.