STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

RTOS (freertos) debug support over STM32CubeIDE

Dear all, I'm trying to debug FreeRTOS over STM32F7/F3/F4 but I don't get it.With STLINK gdb server debugger, i can debug but only see 1 task in debugger panel.I tried with openOCD but it not works...Anyone do it before?ThanksRegards

JBeca.1 by Associate II
  • 5246 Views
  • 9 replies
  • 1 kudos

Debugging X-CUBE-AWS issues on STM32CubeIDE

I'm trying to debug the default X-CUBE-AWS application on the B-L4S5I-IOT01 dev board, but when I launch the debug configuration in STM32CubeIDE, I get the following error:Break at address "0x80209d8" with no debug information available, or outside o...

x-cube-cellular STM32Cube integration - How?

Hi All,Is there a particular way I should be adding the "x-cube-cellular" zip package to my STM32CubeIDE compiler?I want to ensure I place all of the required folders into their respective folders and set the paths in the project properties correctly...

NW27 by Associate III
  • 1342 Views
  • 1 replies
  • 1 kudos

Failed to start GDB server

I am using a Nucleo F303RE board. And whenever I try to debug in STM32cubemxIDE. It always shows an error for failed to start GDB error.I have updated the ST-Link firmware and also checked my device manager.I have also tried disabling my windows defe...

0693W000001t9LWQAY.png
MPadm.1 by Associate
  • 1158 Views
  • 1 replies
  • 0 kudos

Resolved! DMA using HAL Libary does not appear to be functioning

I'm following this tutorial on DMA (https://www.youtube.com/watch?v=EsZLgqhqfO0) which at the end shows how to set up the DMA peripheral to continuously perform ADC conversions and store the results in a circular buffer.I am using an STM32F051C6 (dif...

0693W000002lioMQAQ.jpg 0693W000002lioHQAQ.jpg 0693W000002lio7QAA.jpg
JWyli.1 by Associate II
  • 4215 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.