STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Cube IDE installation under win7-64 SP1

This issue is all over the internet, and as usual with no good solutions.One of the two files which Cube says is not present actually is in that directory. I am totally stuck, having spent a day on this and downloading all sorts of VC++ redistributab...

0693W00000DpmthQAB.jpg 0693W00000DpmtSQAR.jpg 0693W00000DpnNwQAJ.jpg
PHolt.1 by Senior III
  • 6129 Views
  • 9 replies
  • 0 kudos

My STM32CubeIDE 1.5.0 crashing on startup.

Hello, I have a problem with STM32CubeIDE 1.5.0. After installation first run works just fine, second time I launch the problem it crashes on startup.I reinstalled multiple times and running of it ideas. There's an log file: https://pastebin.com/VtS4...

JZysk.1 by Associate II
  • 2767 Views
  • 4 replies
  • 0 kudos

CanFestival-3 for STM32H755 TPDO problem

hello everyone,I'm trying to import canfestival library in the STM32 project. I'm using STM32CubeIDE as IDE for my project. The library is imported correctly and 90% of functionality works well but I'm not able to set the timing for PDO. In attach y...

0693W00000DqBj8QAF.png 0693W00000DqBjNQAV.png
CCagn.1 by Associate
  • 850 Views
  • 0 replies
  • 0 kudos

How use SRC236 for STM32H753ZI with STM32CubeIDE

I USE STM32H753ZI and I want to oversampling some data. For IT, I use SRC236, but It send me an error. The library seems not to be adapted with the target STM32H753ZI. Has anyone encountered this problem before?Sincerely 

MYESS.1 by Associate
  • 1723 Views
  • 3 replies
  • 0 kudos

STM32CubeIDE 1.7.0 ST-Link Linux

I'm trying to run STM32CubeIDE 1.7.0 on Linux using a ST-Link.It must be said that I'm running Linux in Oracle VM 6.1.26It connects, downloads the firmware, but when debugging it's very slow and keeps reporting a warning message:Warn : keep_alive() w...

EGonc.4 by Associate
  • 686 Views
  • 0 replies
  • 0 kudos

Can't find I/O-Register view in debugging mode!

Hi,Yesterday I even completely deleted and re-install STM32CUBEIDE and install the newest version from official site, but it did not help me.Now I have ST-STM32CUBEIDE-1.7.0 and I can't find I/O-Register view in debugging mode.Could you help me in th...

0693W00000Dq19AQAR.png
DK.7 by Senior
  • 3409 Views
  • 8 replies
  • 0 kudos

Resolved! STM32H7B3I-DK Debugging

Hi I have just received my STM32H7B3I-DK and have plugged a micro usb in STLINK connection. When I build a sample application in CubeIDE and try to launch debugger using the default configuration that seems like a good selection, but the debugger te...

HFara.1 by Associate II
  • 1662 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.