STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! cubeIDE, Corrupted database?

This happened, i am still able to compile and debug code.But all the autocomplete (Ctrl+space), funcion linking (ctrl+ left click) and search tools....all nice coding aid features are gone. what is causing this, is there any way of fixing it without...

0693W00000FCow9QAD.png
Javier1 by Principal
  • 1367 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE and cluster support in the SFR panel view

Hello,I'm updating the STM32G0B1.svd file with the FDCAN RAM message registers because right now they are missing. Since it is a lot of registers arrays and clusters, I was willing to use those keywords in the svd file. However, when trying to debug,...

Kraal by Lead
  • 1676 Views
  • 1 replies
  • 0 kudos

Building .bin file CubeIDE

My CubeIDE project currently builds a debug .elf and I am trying to build a .bin file instead. In order to do this, I researched the forums that say I need to go to project properties: C/C++ Bulild->Settings->Tool Settings->MCU Post Build outputs and...

RKher.1 by Associate III
  • 7012 Views
  • 1 replies
  • 0 kudos

Import from Keil MDK into STMCubeIDE

Hello,I have been trying to import an already-existing project into CubeIDE. This project was created on Keil MDK. So, when I import the project, CubeIDE does not recognize the drivers for the board I am program, nor the source files. How can I use t...

BRodr.3 by Associate III
  • 20162 Views
  • 27 replies
  • 1 kudos

How to debug STM32IDE?

Hi. i'm beginner this field and researching for UWB system. so i bought the decawave product to get channel impulse response raw data.​Decawave provides an example, and the example is executed on stm32cubeide. so i installed some software and use the...

0693W00000FClisQAD.png
HJung.3 by Associate II
  • 1343 Views
  • 1 replies
  • 0 kudos

Resolved! Kernel not starting

Hi all,I am pretty new to the STM32 world and I have just started to play around with the STM32F429 discovery kit and STM32CubeIDE. I am OK with the basic & introductory projects, and I was able to have basic IO operations like LED blinking run prope...

DK.9 by Associate II
  • 8813 Views
  • 7 replies
  • 0 kudos

Is it possible to import Makefile in STM32CubeIDE?

I have a C project which is developed outside of STM32Cube IDE. The project contains Makefile.It will be very good to just import the entire project in STM32Cube IDE and compile using the existing Makefile as a part of a bigger project which is alrea...

MDrob.1 by Associate
  • 2744 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.