STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE 1.9.0 released

STM32CubeIDE 1.9.0 was released today on st.com as well as an in-tool update patch.Caution: The in-tool update does not allow updating debug probe drivers and ST-LINK server tool. Full installer is required for this.What is new in 1.9.0?Target suppor...

How to configure SMBUS in stm32h7?

Hello,I am working on Nucleo-h745ziq board.I have to configure the ADM1032 which is temperature sensor and SMBUS compatiable IC.How I can configure the SMBUS in STM32CUBIDE.Which libabry that I have to use.Can you help me.

MDeva.1 by Associate II
  • 3444 Views
  • 6 replies
  • 0 kudos

STM32F4 tick source

Hello,I'm wondering what is general criteria to set a tick source?for example I have two different boards NUCLEO-64 based on STM32F411 and STM32F429I-DISC1 and when i tried to generate a project using the STMCubeIDE, the tool used TIM6 as a source of...

MFawzy by Associate III
  • 2458 Views
  • 1 replies
  • 0 kudos

Can't upload to STM32G030F6P6

Hello,I am working on a custom board using the STM32G030F6P6 chip and I am having trouble connecting to and programming the chips over SWD. I am unable to program the chips from CubeIDE and CubeProgrammer.CubeIDE gives the error message:Error in init...

GJohn.4 by Associate II
  • 2006 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE import/export multi core projects

Hi everyone,I have a project for a dual core microcontroller (STM32H755) in CubeIDE structured as follows. I'm trying to export and import it to another CubeIDE via the import/export functions but I can never get it to import correctly.Does anyone ha...

0693W00000JOG1dQAH.jpg
FBena.1 by Associate II
  • 5961 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.