STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Stlink GDB server source code

Hi, I see the stm32cubeide calls st-link_GDB_server binary program included with the IDE.I can't find the source code for this program which is based on GDB ( GPL). I checked the St GitHub repos and I was unable to find it.The st-link project include...

EGho.1 by Associate
  • 1402 Views
  • 1 replies
  • 1 kudos

Is it possible to add asan library to STM32CubeIDE?

Hi. I am working on a very large project, and recently I discovered that I probably have a buffer overflow issue (a strange error that disappears after commenting a completely unrelated piece of code).I tried many things already, but nothing worked. ...

How do you change an ADC channel at the low level

Hello, I am working with the low level drivers and trying to configure an ADC to read 2 channels via the Cube IDE. I am triggering the read of the ADC via a 1 ms internal timer interrupt. Note I am trying to do this read via polling and not via inter...

SJohn.5 by Associate II
  • 4581 Views
  • 3 replies
  • 0 kudos

Compiler optimization does not produce correct code

Hi there,I have encouraged a strange behavior inside newlib_lock_glue.c.On few devices the code does note execute correctly when the optimization is turned on.To me it looks like the optimization throw away the return and just continue evaluating. th...

0693W00000UokFgQAJ.png 0693W00000UokG5QAJ.png
Fero by Associate II
  • 2646 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.