STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Setup stm32cubeide on mac

I have tried many times to download installer, but each time mac says like 'this is a unverified source you can't open it'. Can you help me to overcome this trouble?

ky1 by Associate
  • 1096 Views
  • 0 replies
  • 0 kudos

can't decrease SPI baud rate

Hİ, i use energy meter ic name is atm90e26 which communicates over SPI and UART. I prefer SPI in my project. But there is a problem about baud rate. Max baudRate of energymeter is 160k bit. Minimum baudRate of stm32g491 is 664k bit at 170Mhz Clock fr...

yasin by Associate
  • 3844 Views
  • 3 replies
  • 0 kudos

Lab 7 for STM32C031C6T6

In Lab 7 at time 17:28 it refers to moving startup code from FLASH to RAM. This is to use RAM for some of the initialization and callback routine. It says to write the following script "After */Drivers/*(.text*) define for initialization - line 74*ma...

hwood1 by Associate
  • 1345 Views
  • 0 replies
  • 0 kudos

NucleoG474RE CAN Receive buffers not receiving any values

I am trying to transmit and receive values from a Sensor connected to NucleoG474RE. The Sensor works with an extended ID (29 bits). I flashed my program onto the board and I am not able to see any return values on my RxData on my debug session of STM...

swedha44 by Associate
  • 924 Views
  • 0 replies
  • 0 kudos

newlib/malloc locking mechanism to be thread-safe

Several users have over the years rightfully complained about newlib/malloc not being thread-safe. This problem does not present itself until the code is executed on target and is quite difficult to debug.Below we will show a solution for this, but f...

STM32CubeIDE Multi-Threaded support

The STM32CubeIDE does not always correctly generate/regenerate the Multi-Threaded support code and ThreadSafe folder.I noticed this when converting an existing project to use FreeRTOS. After experimenting, it seems that if the project contains virtua...

DRega.1 by Associate III
  • 2234 Views
  • 1 replies
  • 0 kudos

Resolved! Cannot connect to Nucleo 144 using ST-LINK

I've installed STM32CubeIDE and the ST-LINK/V2-1 driver. I'm attempting to connect to a Nucleo U5A5ZJ-Q board.When I try to run example code I receive the message: "No ST-LINK detected..."I have removed the jumper on CN4 as instructed if using Nucleo...

STM32CubeIDE debugger skips all breakpoints. (SOLVED)

Hello! I am using STM32CubeIDE Version 1.12.1 and the HAL library with a NUCLEO-F103RB.During debugging the integrated STM32CubeIDE debugger pauses at the first command, in my case at HAL_Init(), but then skips all other breakpoints. The menu option ...

Kmax18 by Senior II
  • 1428 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.