2023-07-23 6:01 PM - edited 2023-07-23 8:29 PM
I am trying to transmit and receive values from a Sensor connected to NucleoG474RE. The Sensor works with an extended ID (29 bits). I flashed my program onto the board and I am not able to see any return values on my RxData on my debug session of STM cube IDE. I tried sniffing the CAN bus through PCAN and discovered that my sensor is responding. I think there is a problem with my Configuration filter but I am not able to decode it. I am a beginner in this and would like a walk through on how to configure this filter to receive values on my buffer. If this is not the problem, I also believe my interrupt is not being called. I do appreciate some help. Thank you.
Edit : I just figured out that my interrupt is not being fired. I have enabled the interrupt line too and called back my RxFifo function. Nothing seems to work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.