STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Issue with ST VSCode STM32 extension.

Hello, I have been using the VSCode STM32 extension on my project for some time and it has been working well. Today, I was doing some major refactoring of some of the code, and this required deleting one of the files no longer required. Unfortunately...

SidPrice by Associate III
  • 3448 Views
  • 3 replies
  • 0 kudos

Resolved! Different optimization level and different assembly code

I have following code snippet, when I compile it with -O0 optimization level it gives below assembly code and I can observe value address on Expression window. But when I compile it with -O3 optimization level I couldn't observe address of value. Whe...

lre1_0-1705427650708.png lre1_3-1705427765575.png lre1_5-1705427949908.png lre1_4-1705427909358.png
lre.1 by Associate II
  • 1837 Views
  • 2 replies
  • 4 kudos

How to solve HardFault_Handler problem at debugging?

Hi Everyone,I am newbie in embedded software field, Just graduated from college.I am trying to connect a SD card and read&write data. I did same things to my STM32F429 but when I tried them on STM32F030C8, I am facing with Debug Current Instruction P...

volkan__0-1705416648469.png
volkan_ by Associate II
  • 4144 Views
  • 3 replies
  • 3 kudos

program Make not found in PATH

Hello Everyone, got an error when i build my project error :- Program "make" not found in PATHi cross check properties and i put the address where all makes are located.despite of doing this get the same error when build the project  

Screenshot (22).png

Resolved! CubeIDE unmet dependencies on Ubuntu are old versions.

Cannot install on Ubuntu 23.10. This release of Ubuntu comes with libncurses6 and libpython3, which are installed on my system. Using the .DEB release downloaded from https://www.st.com/en/development-tools/stm32cubeide.html.EDIT: Tried with both Way...

HAL_FDCAN_ERROR_NOT_INITIALIZED Error

void MX_FDCAN1_Init(void){/* USER CODE BEGIN FDCAN1_Init 0 *//* USER CODE END FDCAN1_Init 0 *//* USER CODE BEGIN FDCAN1_Init 1 *//* USER CODE END FDCAN1_Init 1 */hfdcan1.Instance = FDCAN1;hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;hfdcan1.Init.Mo...

Resolved! I tried to check the operation using "Master Clock Output1" of "RCC", but a timeout occurred and the

Hello everyone in the community. ■What you want to doI want to check the waveform of the signal output using "Master Clock Output1" of "RCC"■Problems occurring:I tried to check the operation using "Master Clock Output1" of "RCC", but a timeout occurr...

toka_1-1705027706388.png toka_2-1705027775016.png toka_3-1705027828466.png toka_4-1705027923134.png
t-oka by Associate III
  • 2249 Views
  • 2 replies
  • 1 kudos

Make digital signal offset-free

I have converted an analog signal with offset voltage through ADC to digital. Now I have an array of 1024 integer values. To edit this signal further, I need to convert the integer values to float. Then make this signal offset-free (by q15). I would ...

Sax by Associate III
  • 1423 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.