STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1708 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 648 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE ignoring include path

I having trouble with the include path of the compiler.I have a header file that is outside my projecto folder, main.h (this was imported from the 1_Image_BFU example). And the header cannot find the header  inside my project even though I have inclu...

leandrospte_0-1711388847676.png leandrospte_1-1711389164641.png leandrospte_2-1711389306504.png

Resolved! Problem with FreeRtos in TrustZone enabled

Hi Hi We are using product STM32H56 series , I am encountering problem while building my project I am using STM32cubeIDE , trust zone enabled .I enabled X-CUBE-FREERTOS  M33non secureIn software package I installed   -STm X-CUBE-FREERTOS  -CMSIS RTOS...

Kendall7_0-1711444735447.png Kendall7_1-1711444777776.png
Kendall7 by Associate II
  • 2731 Views
  • 3 replies
  • 0 kudos

STM32F401RCT6 EEPROM Emulation

Hi,I need to use EEPROM Emulation for my project's needs. I'm using STM32F401RCT6. I tried to use EEPROM emulation in STM32F40x/STM32F41x microcontrollers (AN3969) but after several tries, I only got errors as screenshot at below:Any help would be ap...

omeraydin_0-1694421990342.png

STM32L476 EEPROM Emulation

I have followed the eeprom emulation described in X-CUBE-EEPROM expansionhttps://www.st.com/en/embedded-software/x-cube-eeprom.htmlBut the solution was written using the old STM32 standard API. Does somebody knows about an EEPROM Emulation solution t...

RLeva.1 by Associate
  • 5066 Views
  • 2 replies
  • 0 kudos

Resolved! Power Regulator Voltage scaling and SysClock issue

Hello,I am using STM32H755 microcontroller and STM32CubeIDE V1.13.0 for my development.I am not able to set the clock frequency to 480MHz. Whenever I do so, I receive power regulator voltage scaling error. (Shared in the attachment).The product revis...

HDesa.1 by Senior
  • 5440 Views
  • 6 replies
  • 3 kudos

IOC project doesn't render completely in CubeIDE

After 100 attempts to open the IOC project inside the CubeIDE it opened but only a half, which makes it unusable, what can I do?CubeIDE/Java is eaten all my CPU, but they aren't doing any useful work, help please! 

Captura de pantalla de 2024-03-25 21-51-51.png
XR.1 by Senior
  • 1161 Views
  • 0 replies
  • 0 kudos

Trustzone: NonSecure_Init does not start the nonsecure

Whilst using the standard code generated through cubemx for Trustzone on the Nulceo-WBA55cg Board with TZEN = 1 and having the nonsecure in the Debug configuration of the secure the code doesnt complete the Nonsecure init in the last Line. I checked ...

Isko by Associate II
  • 1680 Views
  • 1 replies
  • 0 kudos

Convert Integer to float

Hello everyone, can someone tell me why casting doesn't work. I want to convert int values of an array to float.for (int i = 0; i<= adcBufferSize; i++){adc_buffer_float[i] = (float)adc_buffer [i];}

Sax by Associate III
  • 8721 Views
  • 12 replies
  • 2 kudos

Resolved! Include not works in STM32CubeIDE

STM32CubeIDE Version: 1.14.0 Build: 19471_20231121_1200 (UTC) OS: Windows 10, v.10.0, x86_64 / win32 Java vendor: Eclipse Adoptium Java runtime version: 17.0.8.1+1 Java version: 17.0.8.1include setupand the exported xml content<option IS_BUILTIN_EMPT...

sayhi2008_0-1710982545148.png
sayhi2008 by Associate II
  • 2758 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.