STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

ADC1 DMA stops TIM3 Global Interrupt

In a project built using STM32F103, I have used TIM3 for some of my frequent tasks (like LED blinking and setting some flags etc.), which work perfectly. Today when I tried to enable ADC1 using DMA Circular, it looks like the TIM3 Global Interrupt ha...

technofection_0-1730645871316.png technofection_1-1730645962615.png technofection_2-1730645984054.png

STM32CubeIDE failed to import examples on Linux

Hi,I'm using STM32CubeIDE on latest Ubuntu:STM32CubeIDE Version: 1.14.1, Build: 20064_20240111_1413 (UTC).If I try to click "Import STM32Cube example", it shows next window with "target selection" which always fails (can only cancel, no selection pos...

STM32CubeIDE linux.jpg
Lex by Associate III
  • 3533 Views
  • 5 replies
  • 0 kudos

HOWTO: Saving versions of a project using git

I had an issue, that i could not reproduce, because i could not restore the exact state of the project. The CubeIDE has its own version control for each file, which is of no great use, since the project consists of many files. Because of that i devel...

Tobe by Senior III
  • 2207 Views
  • 0 replies
  • 0 kudos

Resolved! CubeMX behavior when open from CubeIde.

Hi all!,I notice a different behavior from CubeMX, when starts alone or is called from CubeIDE.When I open CubeMX without CubeIDE, it works as espected. But when CubeMX is open from CubeIDE, it works in a strange way. Per exemple, when I try to put a...

JAlca_0-1730536844987.png JAlca_1-1730536935702.png JAlca_2-1730537000276.png JAlca_3-1730537019658.png
JAlca by Senior
  • 2029 Views
  • 3 replies
  • 1 kudos

stm32cubeIDE project configuration using CLI

Hi. I'm aware that there's a cli tool called  STM32CubeCLT which is used for building programs for stm32 MCUs. But, is there any way that we can ask stm32cubeIDE to perform the following steps?install/remove a certain cmsis-packconfigure a certain pr...

Resolved! Stm32h753i-eval2 USB Host FS

Hi, I need help generating an .IOC file through the cube generator. What I need is USB Host FS. I'm having trouble getting it to work, specifically, there's no voltage on the VBUS output.I want to mention that I was able to create a USB Host HS that ...

ikogman by Associate II
  • 7002 Views
  • 10 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.