2024-07-24 1:19 AM - edited 2024-07-24 1:19 AM
Why is this error very hard to find?
I cannot find the exact reason this is happening?
I have project say named Project_1 that works properly (This is created using TouchGFX on STM32H735G- DK board)
now if i copy this project manually and paste it in another dir and open that in Stm32cubeide and try building
building works once for second time the error occurs
I also tried copying my project codes after crteating a new project using touchgfx instead of just copying existing project
still same error
Note that i have my own files in separate folders that i added in all the projects
after cleaning the project - 1st time build ok - 2nd time same error
I also tried copy pasting the main.d file from my Project_1 into the new project but same error
STM32CubeIDE
Version: 1.16.0
Build: 21983_20240628_1741 (UTC)
STM32CubeMX - STM32 Device Configuration Tool
Version: 6.12.0-RC9
Build: 20240628-1431 (UTC)
Solved! Go to Solution.
2024-08-12 9:12 PM
I found the Cause for the `Application/User/Core/main.d:1: *** multiple target patterns. Stop.` error.
It was because of multiple inclusions of the header files.
I was including all the needed header files for the c files inside its h file this caused the error when the project grew.
Now i changed it into the source files so now the error is gone.
2024-07-24 2:55 AM
* Check if path contains spaces or weird characters
* Delete all *.d files in pre-build step ?
2024-08-12 9:12 PM
I found the Cause for the `Application/User/Core/main.d:1: *** multiple target patterns. Stop.` error.
It was because of multiple inclusions of the header files.
I was including all the needed header files for the c files inside its h file this caused the error when the project grew.
Now i changed it into the source files so now the error is gone.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.