2021-02-04 3:38 AM
Hi All,
I am new to the IDE Cube and I would like to know what is the most appropriate method to add an SPI to an existing Cube project ?
I am specially interested in the people counter firmware running on the Nano boards, to witch I am not able to add an SPI.
The device configuration tool does not open with the code provided by ST .
Adding the files manually, runs into a lot of problems.
Thank you in advance,
Cristian
2021-02-04 12:30 PM
Do you mean STSW-IMG010 software? Whcih comes with an NucleoF401RE_53L1_Expansion.ioc file? What exactly did you try and want to achieve?
2021-02-04 12:40 PM
Yes, it is about STSW-IMG010 .
I need to send over the SPI1 the counting number. I just need to initialize the SPI1 but I'm not able yet to make it work.
I am new to Cube IDE and it seems that I am missing something....
Cristian
2021-02-04 12:49 PM
I get the ERROR:
C:/Users/RFLab/STM32CubeIDE/workspace_1.4.0/en.STSW-IMG010/Src/main.c:250: undefined reference to `HAL_SPI_Transmit'
I read on the web that it could be related to a "c" file that is missing or not in the correct path....
Please see attached the code:
Thank you,
Cristian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.