cancel
Showing results for 
Search instead for 
Did you mean: 

When the file is too large, stmclang may freeze or fail when formatting code.

brucegong
Associate III

Linux VM 6.17.0-7-generic #7-Ubuntu SMP PREEMPT_DYNAMIC Sat Oct 18 10:10:29 UTC 2025 x86_64 GNU/Linux

vscode 1.106.3

Only the ST plugin package is installed, without the Microsoft C++ plugin or clangd.

 

The formatting function is not working properly. The attachment is the result formatted using the Microsoft C++ plugin (only the Microsoft plugin) on Windows.

1 REPLY 1
Cartu38 OpenDev
Lead III

@brucegong 
See https://community.st.com/t5/stm32cubeide-for-visual-studio/code-formatting-style/td-p/853625 possibly.
If formater not functional let's configure VSCode - relying on extra extensions possibly -  the way you want to get it up & running.
While discussing about formater feature marketplace is your friend.
If clang* has some limitation let's report to proper community (LLVM project) and point us the issue report link for reference it may help this community.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.