2023-09-29 12:20 PM
Just installed the STM32 Extension to VS Code. If I start the MCU-Finder from within the extension, the MCU banner appears and then hangs in that state. If I quit VS Code while the MCU Finder banner is visible, the MCU Finder will then continue loading and then open.
The MCU Selector also hangs within STM32CubeMX. If I quit VS Code, the MCU selector will open.
Any ideas?
I have STM32CubeCLT, STM32CubeMX (6.9.1) , and STMCUFinder (6.0.0) installed. Mac OS 12.6.8 (M1).
Thanks
2024-02-01 11:19 AM
I seem to have a similar problem. When I choose “create a new application” from within vscode (stm extension), stm32cubemx starts but hangs on the start my project… choices. Running outside of the extension it just runs.
2024-04-25 12:37 AM
Still not fixed!
st-stm32cubeclt_1.15.0_20695_20240315_1429-macosx_x86_64.pkg is still not signed!
Stm32CubeMX needs full disk access to run even though it runs fine in STM32Ide.
All in all it is just really poor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.