2025-10-22 11:37 PM
Hi,
The Build Analyzer extension in VSCode consistently crashes when I attempt to open or analyze medium-sized projects. The IDE itself not responsive anymore and the Build Analyzer crash unexpectedly.
Steps to Reproduce:
Expected Behavior:
The Build Analyzer should open and display memory and code size statistics without crashing.
Actual Behavior:
The Build Analyzer crashes or fails to load, making it unusable for project analysis.
Additional Info:
Regards
Uwe
2025-10-22 11:48 PM
Thanks for reporting the issue. We apologize for the inconvenience you faced. Could you please help us reproduce the problem? You are the first to report this, although we have seen some signs of this feature being used.
Thank you!
2025-10-23 12:18 AM
Hi,
gcc is gcc 12.3.1. It's same toolchain as in STM32CubeIde 1.16
Size is 48Mbyte. This same issue with smaller files beginning at ~10Mbyte
No. I can't. This is company internal project.
Regards
Uwe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.