2024-07-05 1:44 PM
I have recently used CubeMX to generate C code for a microcontroller that I have used previously. I decided to generate a project using the new CMake option as I have in the past used the Makefile option and migrated it over to CMake. Truth be told, I do not really know how to use CMake all that well. So if I had just generated a brand new CMake project from CubeMX, how do I use the files it generated to compile a binary? I am using WSL 2 Linux to run commands, any help is greatly appreciated, thanks.
I see there is a CMakePresets.json file, what is that? I want to generate a compile_commands.json for my clangd as well.
2024-07-09 1:24 AM
hi @semmens1
We invite you to build it using the latest version of the VSCode extension which is available on Linux
CMakePresets.json is the file containing presets for build and configuration under VSCode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.