2020-07-13 2:35 AM
According to wiki article https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package#Image_flashing it takes "several minutes" to flash partitions.
Flashing bitbake optenstlinux 2.0 (distribution package) or starter image to SDCard of my STM32MP157c-DK2 board takes several hours (~4h)! Is this normal?
2020-07-29 4:01 AM
Hi FOrtn.1,
I can say that this is related to the image size and the used protocol. For example for flashing an image of 1GB it is normal to take a good while. Also via USB protocol would be much faster than via UART.
So I would say this seems normal as long as you obtain a successful flashing.
Please don't hesitate to share more feedbacks in the future.
-Imen
2020-07-29 5:48 AM
Hi,
4 hours sound very long and not normal.
Please check you are not using USB 1.x (12Mbit/s) for whatever reason (e.g. very old USB hub, cable issue, DFU driver issue, etc...).
You could then try using a different SD-Card brand.
Starter kit v2.0.0 image programming on STM32MP157C-DK2 take about 8 minutes on my W10 Laptop using CubeProgrammer v2.5.0. This is about 1.5MB/s average.
Usually similar time or slightly faster when using CubeProgrammer on Linux (or Virtual Machine).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.