2025-10-08 4:33 AM - last edited on 2025-10-21 2:48 AM by Amel NASRI
When a STM32MP2 is "USB/UART for programming" mode i.e. all boot switchs off.
I am running Ubuntu
This happens:
STM32_Programmer_CLI --list
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
===== DFU Interface =====
Total number of available STM32 device in DFU mode: 1
Device Index : USB1
USB Bus Number : 003
USB Address Number : 006
Product ID :
Serial number :
Firmware version : 0x0110
Device ID : unknown
You can't flash it.
When you try you get this error?
Error: TSV files are only supported for STM32MP
The problem at appear to be
https://github.com/fwupd/fwupd
sudo systemctl stop fwupd
This will help how (it may restart)
dmesg showed [ 5746.249668] usb 3-5: usbfs: process 30885 (fwupd) did not claim interface 0 before use
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.