2021-06-16 4:46 AM
I want to use the STM32CubeIDE to debug the M4 on the STM32MP1.
I setup the debug setting for debug probe ST-Link (OpenOCD). If I use the automated generation of the script, it refer to [find target/stm32mp1x.cfg].
This is not part of the default installation of STM32CubeIDE 1.6.1 and it is not located in
https://github.com/STMicroelectronics/OpenOCD/tree/openocd-cubeide-r3/tcl/target
In general it doesn't seems to be the MP1 openocd files for the MP1 within the windows installation.
2021-06-22 7:25 AM
Hi Steffen Rose (Community Member),
[find target/stm32mp1x.cfg] called from the project debug script is indeed part of the installation of STM32CubeIDE1.6.1
<CubeIDE Install dir>\plugins\com.st.stm32cube.ide.mpu.debug.openocd_xx\resources\openocd\st_scripts\target
Did you install the IDE from this repository?
Regards,
Olivier
2021-06-22 8:26 AM
Yes, I did install the official release from ST.
But thank you for your path. It seems my mistake was, that I searched in the *mcu* and not in the *mpu* path of openocd.
I'm unsure, why the user script this not do automatically. But it help's me.
Thank you
Regards
Steffen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.