2020-10-31 4:41 PM
STM32MP157c-EV1 is connected with two QSPI NOR flash chips.
When programming NOR flash using the CubeProgrammer using tsv file, it automatically programs the two NOR flash in Dual-Flash QSPI mode.
My requirement is to program just the Single Flash chip connected to BK1.
how can I tell the CubeProgrammer to do this?
2020-11-09 6:37 AM
Hi All, I am still stuck on this, any help is much appreciated.
I got my A7 custom boot loader working, able to boot and ready to copy the M4 firmware stored in Single External NOR Flash and load in the memory,
The issue I have is Cube Programmer storing the M4 firmware in two Flash devices in dual-flash qspi mode.
I need to find a way to store the M4 firmware in signel flash device using CubeProgrammer and tsv file
2020-11-25 6:24 AM
Hi @BalaGajenthan ,
I have several question to help me to understand the context :
Thanks !
BR,
Christophe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.