2022-01-16 11:45 PM
Good afternoon.I tried to create a demo project (STM32MP157C-DK2\Demonstrations\Al_Character_Recognition) for the STM32MP157D_DK1 board. When assembling, I had a problem.(Gluk_test_1) How to include the library in the project correctly? Sincerely, Alexander.
2022-01-16 11:47 PM
Is your question "how to include any library"? or "how to include a particular library you cant find"?
2022-01-16 11:51 PM
2022-01-17 4:04 AM
Dear @Vlaty.1 ,
This link from community could help you:
https://community.st.com/s/question/0D50X0000BJ2gL4SQJ/how-to-add-external-libraries-in-stm32cubeide
SofLit
2022-01-17 10:59 PM
Thanks for the information. This is what I need. Sincerely, Alexander.
2022-01-19 8:01 AM
Thank you for the feedback.
Please close this post by clicking the "Select as Best" button in the above answer. This will help other community members to find the solution more quickly.
Thank you.
2022-01-25 10:44 PM
Good afternoon. Thanks for the help. But, unfortunately, the problems remained. I really need an example of working on STM32MP157D-DK RTC and working with a graphical application. I tried to make an example of using RTC myself. But, unfortunately, it works once. I used python 3. Where did I go wrong? Sincerely, Alexander.
2022-01-26 12:26 AM
Hello,
Did you succeed to link the library? you said "But, unfortunately, it works once", so I think yes.. and you have another issue ..
SofLit
2022-01-26 1:19 AM
2022-02-09 1:39 AM
Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong?
Sincerely, Alexander.
//////////////////////////////////////////////////////////////////////////////
def time_show():
await asyncio.sleep(10)
os.system("date > time_info.txt")
f = open('time_info.txt','r')
read_data = f.read()
f.close()
os.system("rm time_info.txt")
print(read_data[11],read_data[12],read_data[13],read_data[14],read_data[15])
if __name__ == "__main__":
loop = asyncio.get_event_loop()
loop.run_until_complete(time_show())
datsa = 10
for i in range(data):
time_show()
os.system("python3 tablo")
//////////////////////////////////////////////////////////////////////////
import asyncio
import datetime
import os
import subprocess
import time
def display_date(end_time, loop)
print(datetime.datetime.now())
if (loop.time() + 1.0) < end_time:
time.sleep(60)
loop.call_later(1, display_date, end_time, loop)
else:
os.system("python3 time_date1")
loop = asyncio.get_event_loop()
end_time = loop.time() + 5.0
loop.call_soon(display_date, end_time, loop)
loop.run_forever()
loop.close()
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.