2021-09-13 2:38 AM
I am trying to Debug m4 in production mode. M4 is not halted.
I am getting an error "Failed to insert breakpoint".
I can successfully debug in Engineering mode. but, I need to Debug in Production mode.
Can you explain how to solve this issue?
2021-09-14 4:56 AM
Hi @JSIGA.1 ,
Debugging in Production mode may present some pitfalls ...
Which IDE are you using ? I presume STM32CubeIDE ?
If not already done I recommend you to make a trial with a provided Cube exemple as per described here:
You have to take care if Linux is properly booted and if ethernet and UART/STLink are all functionnals.
Hope it help
Olivier
2021-09-14 5:45 AM
hello,
I am using STM32IDE v1.7.0 on UBUNTU 20.04.
I can communicate with UART from IDE. when I try to debug, M4 files are sending to Linux using SSH and then I got the error "Failed to insert breakpoint".
Joshiga
2021-09-14 7:56 AM
Hello @JSIGA.1 ,
Are you able to suspend M4 program?
Could you send us the debug console output to better understand?
Thanks for your feedback,
Ludovic
2021-09-15 1:54 AM
Hello @LudovicR
Below is my console output,
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J8M3B5S1 (API v3) VID:PID 0483:374F
Info : Target voltage: 3.804917
Info : clock speed 8000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : STM32MP157AACx.cm4: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157AACx.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157AACx.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : STM32MP157AACx.cm4: external reset detected
Info : starting gdb server for STM32MP157AACx.cpu0 on 3334
Info : Listening on port 3334 for gdb connections
Info : starting gdb server for STM32MP157AACx.cm4 on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP157AACx.cm4:
Info : New GDB Connection: 1, Target STM32MP157AACx.cm4, state: reset
Warn : GDB connection 1 on target STM32MP157AACx.cm4 not halted
Warn : negative reply, retrying
Warn : negative reply, retrying
Info : accepting 'gdb' connection on tcp/3333
Info : Halt timed out, wake up GDB.
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP157AACx.cm4:
Info : New GDB Connection: 2, Target STM32MP157AACx.cm4, state: reset
Warn : GDB connection 2 on target STM32MP157AACx.cm4 not halted
Warn : negative reply, retrying
Warn : negative reply, retrying
Warn : target STM32MP157AACx.cm4 is not halted (add breakpoint)
Error: can't add breakpoint: target running
Info : dropped 'gdb' connection
shutdown command invoked
Info : dropped 'gdb' connection
I am using
STM32cubeIDE 1.7.0 on UBUNTU 20.4
OpenSTLinux SDK openstlinux_5.10_dunfell_mp1_21_03_31
How can I overcome this issue?
2021-09-15 6:59 AM
Hello @JSIGA.1 ,
It seems you are not using an ST Board, since it is connected with ST-Link v3 and target voltage seems high but it is not the problem I guess here. A recommendation could be to reduce the clock speed during first runs.
But main point is that Cortex-M is in reset mode, so GDB server is not able to attach to it.
A first test could be to load your M4 firmware "manually" through Linux console running script located into /usr/local/projects//fw_***.sh or directly with remoteproc framework command. Note that an infinite loop is needed inside your M4 firmware...
If it succeed, then create a new debug configuration, duplicating your production mode debug configuration, but without any download: set-up in Startup tab, disable download from your elf.
This will allow to take control with GDB server.
Let me know if it helps.
LudovicR
2021-09-16 1:59 AM
Hello @LudovicR ,
Yes Ludovic, I am using a customized module based on STM32mp157 .
I've tested your suggestion. Now I could degub the M4 while A7 is alive.
Thank you so much for your help.
Js
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.