2025-08-12 1:07 AM - last edited on 2025-08-12 3:16 AM by Andrew Neil
Hi there,
I'm working on a STM32MP135 project.
I'd like to see some information on the Build Analyzer and/or Static stack analyzer but they always report the grids empty.
The project is compiled with the -fstack-usage and debualt Debug level (-g).
I checked that for each source files of the project are generated the .cyclo, .su, .d and .o files in the Debug directory.
The analyzers windows do not have a button to associate the project: but it seems not to be a problem with the latest relases.
So, why I cannot browse the analyzers data?
Version: 1.19.0
Build: 25607_20250703_0907 (UTC)
Thanks, regards
Solved! Go to Solution.
2025-08-13 3:36 AM
2025-08-12 6:44 AM - edited 2025-08-12 6:58 AM
I've found that 'sometimes' works the 'Refresh' button .. sometimes .. the binaries are always rebuilt.
2025-08-13 3:36 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.