2025-02-14 2:54 AM - edited 2025-02-14 2:55 AM
Hi,
I'm trying to import an ioc file for STM32MP257f-ev1. The original project was build on CubeMx 6.13 for MAC-OS using FW_MP2_V1.0.0 and I'm using CubeMx 6.13 under linux. When I open the .ioc file, It asked me if I want to migrate to FW_MP2_V1.1.0 or continue with the current version. If I choose to migrate everthing goes fine, but I continue with current package version CubeMX stack during the "Render UI" progress bar phase.
Could someone help me?
Marco.
This is got the error log I got on terminal:
Solved! Go to Solution.
2025-08-22 12:06 AM - edited 2025-09-04 6:52 AM
I get exactly the same error when trying to open a project on STM32F103CBT6 version 6.13.0 in cube 6.14.0, 6.14.1, 6.15.0.
PA11.Locked=true
Mcu.Pin17=PA11
2025-08-22 12:06 AM - edited 2025-09-04 6:52 AM
I get exactly the same error when trying to open a project on STM32F103CBT6 version 6.13.0 in cube 6.14.0, 6.14.1, 6.15.0.
PA11.Locked=true
Mcu.Pin17=PA11
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.