2024-11-07 9:24 AM
Hello,
I am working with the STM32MP257F-EV1 on version 1.16.0 of CubeIDE. Specifically I am following the guide laid out in this link: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Develop_on_Arm%C2%AE_Cortex%C2%AE-M33/Modify,_rebuild_and_reload_the_firmware
I am trying to run the debug but when I do I get the following output:
Open On-Chip Debugger 0.12.0+dev-00597-ga5a21219f (2024-06-03-11:02) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J15M7B5S1 (API v3) VID:PID 0483:3753
Info : Target voltage: 3.284210
Info : Unable to match requested speed 5000 kHz, using 3300 kHz
Info : Unable to match requested speed 5000 kHz, using 3300 kHz
Info : clock speed 3300 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : [STM32MP257FAIx.ap0] Examination succeed
Info : [STM32MP257FAIx.m33] Cortex-M33 r1p0 processor detected
Info : [STM32MP257FAIx.m33] target has 8 breakpoints, 4 watchpoints
Info : [STM32MP257FAIx.axi] Examination succeed
Info : gdb port disabled
Info : starting gdb server for STM32MP257FAIx.axi on 3334
Info : Listening on port 3334 for gdb connections
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : gdb port disabled
Info : starting gdb server for STM32MP257FAIx.m33 on 3333
Info : Listening on port 3333 for gdb connections
Info : gdb port disabled
Info : [STM32MP257FAIx.m33] external reset detected
Info : accepting 'gdb' connection on tcp/3333
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP257FAIx.m33:
Info : New GDB Connection: 1, Target STM32MP257FAIx.m33, state: reset
Warn : GDB connection 1 on target STM32MP257FAIx.m33 not halted
Info : accepting 'gdb' connection on tcp/3333
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32MP257FAIx.m33:
Info : New GDB Connection: 2, Target STM32MP257FAIx.m33, state: reset
Warn : GDB connection 2 on target STM32MP257FAIx.m33 not halted
Error: [STM32MP257FAIx.m33] not halted
Error: [STM32MP257FAIx.m33] context restore failed, aborting resume
Info : target STM32MP257FAIx.m33 was not halted when resume was requested
Info : Halt timed out, wake up GDB.
Error: [STM32MP257FAIx.m33] not halted (gdb fileio)
Does anyone know why I'm getting this output and what could be causing it? Thanks,
Carson
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.