STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32MP15 ECO 5.0.0 Kernel boot Unhandled fault: imprecise external abort (0x1c06) [cut here]

ECO sources used (not git). Custom board based on STM32MP157AAA3.Both when using OPTEE in DDR and SRAM this issue occurs.The kernel reports an "cut here" and then reports:[ 0.273935] Unhandled fault: imprecise external abort (0x1c06) at 0x97638f7aThi...

debugging_0-1697037001071.png debugging_0-1697106719761.png

STM32 MP157 SSH Debugging

Hello, I currently working with a STM32MP157D-DK1 Development Board. I populated the board with a prebuild openstlinux 6.1 build. A SSH connection via console is successful.To get the M4 microcontroller running I was able to build a .elf file from th...

MHerz.1 by Associate II
  • 5484 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP15 ECO 5.0.0 metadata.bin

The TF-A Makefile.sdk creates a small metadata.bin file for each type of boot (USB, SD-cARD, EMMC)1/ How to generates this outside of Makefile.sdk  ? I use this, but is only generates one file and there seems no parameter for the type of the boot dev...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.