STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32MP257F-DK and CubeMX

STM32MP are not microcontrollers - so moved to the MPU section.Hi,How can I flash a CubeMX generated project to STM32MP257F-DK microcontroller?Do I have to generate a custom Yocto image with custom device tree, where I load the CubeMX generated devic...

fa31 by Associate III
  • 1064 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to change MAC Address on STM32MP1

Hello everyone,I'm currently working with an STM32MP157F-DK2 device, and I need to change the MAC address. I'm building the image using bitbake, but I've encountered an issue when trying to modify the MAC address through OTP cells linkHere’s the outp...

symeon by Associate II
  • 1572 Views
  • 2 replies
  • 1 kudos

ST_Link support in SEGGER EMBEDDED STUDIO

Hello We have a few queries regarding the use of ST-Link for debugging, and I would greatly appreciate your assistance in this matter.We are currently using a J-Link Base probe for debugging the STM32MP157F processor in SEGGER EMBEDDED STUDIO, and we...

Aks by Associate III
  • 6579 Views
  • 5 replies
  • 0 kudos

CubeIDE warnings

Hello,CubeIDE 1.18Half a year now I acknowledge these two warnings (developing for the CM4):It appears all the time when I restart a debug session with a build before. How can I ged rid of that? For the moment I just click always "yes"... Of course I...

EOF_0-1742284925454.png EOF_3-1742285850328.png
EOF by Associate III
  • 636 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE can't setup OpenSTLinux

I've set the root path in the OpenSTLinux SDK manager, but when I try to download scarthgap from the 'install other software' dialog, it appears to download the SDK, but it never shows up. It's not at the path I specified either. I don't know where, ...

BlotCoo by Associate II
  • 1023 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.