2022-10-19 5:26 AM
When we use the PMIC values from DK2 example.
1 . ERROR: regul ldo3: max value 750 is invalid
WARNING: register_pmic:600 failed to register ldo3
PANIC at PC : 0x2fff05cb
2 Next we tried setting the ldo3 max, min values to 3V and 1.8V and it was working fine but had next layer of issue as mentioned below.
NOTICE: CPU: STM32MP157AAD Rev.Z
NOTICE: Model: MelodySOM
INFO: PMIC version = 0x21
WARNING: VDD unknown
NOTICE: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
PANIC at PC : 0x2ffead6d
Exception mode=0x00000016 at: 0x2ffead6d
Requesting for your help to solve this as soon as possible.
2023-09-17 5:12 AM - edited 2023-09-17 5:15 AM
@michiel.tjampens I believe the workshop had multiple nodes in the TF-A DT for power , like vdd_sd etc.. Reduce it to only two nodes. My (perfectly hardware good custom board which has run ECO 1.0 for years) had also this panic in ECO 5.0 and after debugging found it kept crashing in fdt.c on the 3rd node no matter what that node was. I don't have any setting for vtt_dr in then TF-A DT but this board does not use PMIC though.
See my last post in: https://community.st.com/t5/stm32cubemx-mpus/stm32mp15-eco-5-0-0-board-bring-up-panic-with-legacy-power/td-p/585845
2023-09-17 5:25 AM
Hi @debugging , for once the Lab probably was correct. I think in old ECO's that check wasn't there or something. Because both the lab and a ek dts removed the lines in question.
vtt_ddr: ldo3 {
regulator-name = "vtt_ddr";
regulator-always-on;
regulator-over-current-protection;
st,regulator-sink-source;
};Which kinda makes sense because the ldo's voltage is 'fixed' to buck2 divided by 2 when in sink-source.
I'll check your post when I manage to get that far, the voltage error was replaced with addr bus test failure (but that's offtopic).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.