2024-04-17 7:45 AM
Hello,
We are currently in the process of bringing up and industrializing an embedded STM32MP1 board with eMMC as main data storage.
We would like to flash the eMMC via U-boot using a tsv file.
We have a couple of tsv files that are working correctly, but some aren't and it's been really hard (not to say a real pain) to debug precisely the issue of why exactly the file is wrong.
Using the following command : ./STM32_Programmer_CLI -c port=usb1 -d board-emmc.tsv, the error I get is the following :
Error: TSV file proto-new.tsv not conform: it may miss some columns or fields
Error: TSV flashing service failed
This is generic and provides no detailed infos about the actual error.
Is there any tools or ways to further debug tsv files ? Sorry if I'm missing something obvious ...
Quentin
2024-04-17 7:59 AM
Hi @Vauteck
TSV file should only contains tabulation as separators.
More details are available from this wiki page: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout
Best regards,
--JM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.