2026-01-01 6:05 PM
Hello Everyone
linux kernel version: 6.6.78
After configuring the device tree, I can see the SPI device /dev/spidev6.0 on the STM32MP257F-DK board. However, when I run spidev_test[1], it returns the error message "Invalid argument."
I tried using an oscilloscope to measure the signals on the CLK, MOSI, and MISO pins separately, but no signals were detected.
Please give me some suggestions to help me fixed it. Thanks in advance.
//------------------------------------------------------------------------------------------------------
the SPI device tree setting as following:
Path:
~/STM32MPU-Ecosystem-v6.6/Developer-Package/BSP/sources/ostl-linux/linux-stm32mp-6.6.78-stm32mp-r2-r0/linux-6.6.78/arch/arm64/boot/dts/st/stm32mp257f-dk.dts
aliases {
serial0 = &usart2;
serial1 = &usart6;
serial2 = &usart1;
ethernet0 = ð1;
spi6 = &spi6;
};
&spi6 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi6_pins_a>;
pinctrl-1 = <&spi6_sleep_pins_a>;
status = "okay";
spidev@0{
compatible = "rohm,dh2228fv";
reg = <0>;
spi-max-frequency = <10000000>;
};
};
reference:
1.How to use SPI from Linux userland with spidev, https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev.
2026-01-05 7:24 AM
Hello @LeonSu ,
Are you sure you used properly the tool command by using the --device argument ?
If yes, can you share a bit more information about boot logs, and command logs ?
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.