2021-11-25 1:41 AM
When compiling the U-boot, these four commands are used:
PC $& gt; export KBUILD_OUTPUT=.. /build/stm32mp15_trusted
PC $& gt; export DEVICE_TREE=stm32mp157c-dk2
PC $& gt; make stm32mp15_trusted_defconfig
PC $& gt; make all
use the first: export KBUILD_OUTPUT=.. /build/stm32mp15_trusted, the compiler will fail, but if there is no first statement, the compiler will succeed
Solved! Go to Solution.
2021-11-25 4:16 AM
Hello @Ffu.1 ,
The error displayed about "make mrproper", means that your build folder is not clean and was already used with another configuration or with another build directory.
So please, run this command to clean your directory
make mrproperThen redo the commands:
export KBUILD_OUTPUT=../build/stm32mp15_trustedmake stm32mp15_trusted_defconfigAnd specify the device tree in the make all command :
make DEVICE_TREE=stm32mp157c-dk2 allRegards,
Kevin
2021-11-25 4:16 AM
Hello @Ffu.1 ,
The error displayed about "make mrproper", means that your build folder is not clean and was already used with another configuration or with another build directory.
So please, run this command to clean your directory
make mrproperThen redo the commands:
export KBUILD_OUTPUT=../build/stm32mp15_trustedmake stm32mp15_trusted_defconfigAnd specify the device tree in the make all command :
make DEVICE_TREE=stm32mp157c-dk2 allRegards,
Kevin
2021-11-25 7:32 PM
This does work, but why only u-boot.bin is generated, not u-boot.stm32
2021-11-26 2:34 AM
Hi @Ffu.1 ,
Yes, I assume that you are using an ecosystem v3.0.0 or 3.1.0. It is normal that you do not have a u-boot.stm32.
Since the ecosystem v3.0.0, two binaries are needed from u-boot:
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#Output_files
u-boot.dtb and u-boot-nodtb.bin
The .stm32 is now a tf-a.stm32. To learn more things about the FIP, you can read the ecosystem release note: https://wiki.st.com/stm32mpu/wiki/STM32MP15_ecosystem_release_note_-_v3.0.0#OpenSTLinux_-28Cortex-C2-AE-A7-29
or this part of the TF-A overview: https://wiki.st.com/stm32mpu/wiki/TF-A_overview#FIP
The FIP can be generated automatically when you build your TF-A, please have a look to the README.HOW_TO.txt of the TF-A.
Regards,
Kevin
2021-12-01 3:17 AM
Hello @Ffu.1 ,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.