2021-09-14 2:48 AM
Hi all,
How can I create swap partition in STM32MP1?
Previously I did get an answer to how to increase the rootfs size. Any guidance on this will be highly appreciated.
TIA
Solved! Go to Solution.
2021-09-22 9:30 AM
A swap partition is a good idea when you have a real hard-disk or a fast SSD that includes an internal cache.
With SD card or simple flash devices (NAND, SPI, ...) I expect that the write speed will not give you the performance you would expect.
Plus the limited write/erase cycles of flash devices could impact its life-time, when used too often as swap.
Nevertheless if your need is to just use the cache in some "special" and "limited" case, it could still be interesting to turn swap on.
But I don't have clear what is your need?
Some command to create a swap partition from command-line? Or change the flash partition to include a swap when you re-flash the board?
And which storage you plan to use? Hard-disk, SD card, ...?
2021-09-14 2:49 AM
Hi @NPal.2 ,
Could you further elaborate what you mean by swap partition ?
Thanks
Olivier
2021-09-14 2:55 AM
Hi @Oliver
In case of Linux we have : ext4 , boot and swap partition. When system runs low on RAM it takes up memory from swap memory to satisfy those need. I want to create a similar partition.
I hope I was able to provide you some clarity around this.
2021-09-22 9:30 AM
A swap partition is a good idea when you have a real hard-disk or a fast SSD that includes an internal cache.
With SD card or simple flash devices (NAND, SPI, ...) I expect that the write speed will not give you the performance you would expect.
Plus the limited write/erase cycles of flash devices could impact its life-time, when used too often as swap.
Nevertheless if your need is to just use the cache in some "special" and "limited" case, it could still be interesting to turn swap on.
But I don't have clear what is your need?
Some command to create a swap partition from command-line? Or change the flash partition to include a swap when you re-flash the board?
And which storage you plan to use? Hard-disk, SD card, ...?
2021-09-24 7:25 AM
Hi @AntonioST . Thanks for your response. I feel the comments provided by you give me a better insight. I wanted to make a swap partition in case my system runs out of memory, it can pick up some from swap.I plan to use SD-Card.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.