2023-11-28 4:31 AM - edited 2023-11-28 4:38 AM
Hi,
I would like to integrate the STPM4RasPI with MP135F-dk. After following the https://wiki.st.com/stm32mpu/wiki/STPM4RasPI_expansion_board tutorial, I am receiving an error.
Driver is enabled:
STPM4RasPI module is properly attached.
Do you have any possible solutions?
Best,
Jacek
Solved! Go to Solution.
2023-11-29 2:35 AM
Hi @Olivier GALLIEN ,
Instruction given in https://wiki.st.com/stm32mpu/wiki/X-LINUX-TPM_expansion_package was helpful. I had to adjust arch/arm/boot/dts/stm32mp135f-dk.dts as:
&spi5{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi5_pins_a>;
pinctrl-1 = <&spi5_sleep_pins_a>;
cs-gpios = <&gpioh 11 0>;
status = "okay";
st33htpm0: st33htpm@0{
status="okay";
compatible = "st,st33htpm-spi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>; /* CS #0 */
spi-max-frequency = <10000000>;
};
}; And then the module was successfully detected.
Going back into the https://wiki.st.com/stm32mpu/wiki/STPM4RasPI_expansion_board there is a significant difference in configuration:
&spi5{
cs-gpios = <&gpioh 11 0>;
status = "okay";
st33htpm0: st33htpm@0{
status="okay";
compatible = "st,st33htpm-spi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>; /* CS #0 */
spi-max-frequency = <10000000>;
};
}; It is wrong and should be changed.
Best,
Jacek
2023-11-28 4:55 AM
Hi @jschneider
,
Please confirm you are on top of release V5.
For this last release you may also try https://wiki.st.com/stm32mpu/wiki/X-LINUX-TPM_expansion_package which have been validated on DK 135F.
Cross-checking both article and solution may help to find the missing piece
Olivier
2023-11-28 4:59 AM
Hi @jschneider
I also add a big warning : any wrong side connection of the TPM to RasPI connector likely lead to kill the TPM. ( high probability)
Olivier
2023-11-29 2:35 AM
Hi @Olivier GALLIEN ,
Instruction given in https://wiki.st.com/stm32mpu/wiki/X-LINUX-TPM_expansion_package was helpful. I had to adjust arch/arm/boot/dts/stm32mp135f-dk.dts as:
&spi5{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi5_pins_a>;
pinctrl-1 = <&spi5_sleep_pins_a>;
cs-gpios = <&gpioh 11 0>;
status = "okay";
st33htpm0: st33htpm@0{
status="okay";
compatible = "st,st33htpm-spi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>; /* CS #0 */
spi-max-frequency = <10000000>;
};
}; And then the module was successfully detected.
Going back into the https://wiki.st.com/stm32mpu/wiki/STPM4RasPI_expansion_board there is a significant difference in configuration:
&spi5{
cs-gpios = <&gpioh 11 0>;
status = "okay";
st33htpm0: st33htpm@0{
status="okay";
compatible = "st,st33htpm-spi";
#address-cells = <1>;
#size-cells = <0>;
reg = <0>; /* CS #0 */
spi-max-frequency = <10000000>;
};
}; It is wrong and should be changed.
Best,
Jacek
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.