2025-01-20 5:06 PM
I am trying a simple CM33 ELF test. This one just has the STM32CubeMX boilerplate for the CM33 (non secure). I added a toggle on GPIOJ[6].
I stripped out a ton of the inits leaving just the GPIOJ[6] and pin toggle. after the seq below LED3 *does* toggle.
But... the system watchdogs after ~30secs. How to kick off a CM33 program and not have start hang?
Is there some way the CM33 can tell the CA35s to keep going and leave the CM33 running?
echo -n /home/hedley > /sys/module/firmware_class/parameters/path
echo start >/sys/class/remoteproc/remoteproc0/state <<<<<<<< this will not return to the prompt... hang.
/home/hedley
lrwxrwxrwx 1 hedley hedley 27 Jan 20 16:50 rproc-m33-fw -> test_mp2_CM33_NonSecure.elf
-rwxr-xr-x 1 hedley hedley 3216664 Jan 20 16:51 test_mp2_CM33_NonSecure.elf
tnx
Hedley
2025-01-21 12:13 AM
Hi @Hedley,
Such kind of error usually happen when the used OpenSTLinux image does not properly assign resource to M33.
Are you using a custom image or the starter package ?
For starter package you might use the FlashLayout_xxxx_stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-optee
For reference you can refer to Develop on Arm® Cortex®-M33 - stm32mpu
Hope it help
Olivier
2025-01-23 5:22 PM
Appreciate the input Olivier. The reason for the hang is as follows.
1) If you use the hal funcs to init and toggle GPIOJ[6]... the LED will toggle but you will crash for ~30secs till WD reset.
2) If you use the BSP funcs to init and toggle the GPIOJ[6], the CM33 can be started and the kernel doesn't crash.
Make sure the #if DEBUG while(debug) loop is not in or your code will go nowhere. (unless you want to wait for debug attach)
#if 0
#ifdef DEBUG
while(debug);
#endif /* DEBUG */
#endif
Hedley
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.