cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP257F-DK OTG failed to connect iPhone 14

dothanhtrung
Associate

Hi.

 

I am trying to connect iPhone 14 (lightning port) to OTG (CN15) on STM32MP257F-DK, but there is no connection.

  • iPhone 14 is not charged. No USB connection is shown on iPhone.
  • On the board:
    • `lsusb` does not show any new connection.
    • `dmesg` does not show any new log, like there is no new cable plugged at all.

The lightning-to-C cable has been tested with other devices and works fine.

iPhone 16 (type-C port) can connect to OTG to be charged and do USB tethering just fine.

I am already using the newest kernel 6.6.78 from https://github.com/STMicroelectronics/linux, branch "v6.6-stm32mp".


So I would like to confirm if OTG on STM32MP257F-DK support lightning connection or not.

 

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Bossen
ST Employee

Hi dothanhtrung,

 

Let me add the information here for others who encountered same issue.

 

The root cause is the firmware of Cortex-M33 is stopped manually. By default, CM33 FW is loaded automatically thanks to the system services. The CM33 FW manages CC communication of type-C port, as well as the cable detection of USB type-C. When the firmware is stopped, there is no notification to system when USB is attached. No USB is recognized then.

 

Best Regards,

Bossen WU

View solution in original post

2 REPLIES 2
Billy OWEN
ST Employee

Hi @dothanhtrung 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

Bossen
ST Employee

Hi dothanhtrung,

 

Let me add the information here for others who encountered same issue.

 

The root cause is the firmware of Cortex-M33 is stopped manually. By default, CM33 FW is loaded automatically thanks to the system services. The CM33 FW manages CC communication of type-C port, as well as the cable detection of USB type-C. When the firmware is stopped, there is no notification to system when USB is attached. No USB is recognized then.

 

Best Regards,

Bossen WU

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.